2019-02-01 7:37 AM
I don't really understand how to use drawString. The text explaining the function is not very clear in my opinion. And most importantly, it wont draw the string I want it to draw. I'm probably doing something wrong, but I don't know what.
2019-02-02 5:24 AM
Hi @Community member,
Is the same issue you're having in the other post with the ButtonWithIconAndLabel? Can you post your code?
Thanks
2019-02-04 12:46 AM
Yes, it is the same issue.
Here is my own code, based on yours.
In my class:
void PhysicalButton::draw(const Rect& area)
{
/* Draw the icons of the button */
Button::draw(area);
/* Draw the label */
const Font* fontToDraw = _label_txt.getFont();
const Unicode::UnicodeChar * string = _label_txt.getText();
uint8_t textHeightIncludingSpacing = fontToDraw->getMaxTextHeight(string) * fontToDraw->getNumberOfLines(string) + fontToDraw->getSpacingAbove(string);
if ((fontToDraw != NULL) && _label_txt.hasValidId())
{
Rect widgetArea;
widgetArea = Rect(getX(), getY(), this->getWidth(), this->getHeight());
Rect invalidatedArea = Rect(0, this->getHeight() - textHeightIncludingSpacing - 3, this->getWidth(), textHeightIncludingSpacing);
translateRectToAbsolute(widgetArea);
LCD::StringVisuals visuals(
fontToDraw,
_label_color,
alpha,
_label_txt.getAlignment(),
0,
TEXT_ROTATE_0,
_label_txt.getTextDirection(),
0
);
HAL::lcd().drawString(
widgetArea,
invalidatedArea,
visuals,
_label_txt.getText()
);
}
}
void PhysicalButton::Setup(
bool visible,
bool faded,
const uint16_t icon_id,
const uint16_t title_id)
{
int16_t bgX = 0, bgY = 0;
Bitmap bg, icon;
int16_t iconX = 0, iconY = 0;
// _label_txt = TypedText(title_id);
/* The mask determines where the button is being placed*/
switch (_mask)
{
case Mmi::Button::Bit::Masks::Hot : /* TOP-LEFT */
bg = Bitmap(BITMAP_BUTTONBACKGROUND1_ID);
bgY = BG_TOP_Y;
break;
case Mmi::Button::Bit::Masks::Cold : /* TOP-RIGHT */
bg = Bitmap(BITMAP_BUTTONBACKGROUND4_ID);
bgY = BG_TOP_Y;
break;
case Mmi::Button::Bit::Masks::Mix : /* MID-LEFT */
bg = Bitmap(BITMAP_BUTTONBACKGROUND2_ID);
bgY = BG_MID_Y;
break;
case Mmi::Button::Bit::Masks::Jug : /* MID-RIGHT */
bg = Bitmap(BITMAP_BUTTONBACKGROUND5_ID);
bgY = BG_MID_Y;
break;
case Mmi::Button::Bit::Masks::Back : /* BOTTOM-LEFT */
case Mmi::Button::Bit::Masks::ExHot :
bg = Bitmap(BITMAP_BUTTONBACKGROUND3_ID);
bgY = BG_BOT_Y;
break;
case Mmi::Button::Bit::Masks::Menu : /* BOTTOM-RIGHT */
bg = Bitmap(BITMAP_BUTTONBACKGROUND6_ID);
bgY = BG_BOT_Y;
break;
}
/* Set the X pos of the background */
if (_mask & (Mmi::Button::Bit::Masks::Cold | Mmi::Button::Bit::Masks::Jug | Mmi::Button::Bit::Masks::Menu))
{
bgX = 128;
}
else
{
bgX = 112 - bg.getWidth();
}
/* Only if the icon_id is valid load the correct icon into the icon bitmap */
if (icon_id != 0xffff)
{
icon = Bitmap(icon_id);
/* Set the X pos of the Icon */
if (_mask & (Mmi::Button::Bit::Masks::Cold | Mmi::Button::Bit::Masks::Jug | Mmi::Button::Bit::Masks::Menu))
{
iconX = ((3 * bg.getWidth()) / 5) - (icon.getWidth() >> 1);
}
else
{
iconX = bg.getWidth() - ((3 * bg.getWidth()) / 5) - (icon.getWidth() >> 1);
}
/* Y-position always the same */
iconY = ICON_POS_Y;
}
/* Otherwise load an empty image */
else
{
icon = Bitmap(BITMAP_IMG_EMPTY_ID);
}
/* Set all the bitmaps */
setBitmaps(bg, bg, icon, icon);
/* Set the XY coordinates relative to the bg */
setIconXY(iconX, iconY);
/* Set the XY coöordinates */
setXY(bgX, bgY);
/* Set visible */
setVisible(visible);
/* Set faded */
if (faded)
{
setAlpha(64);
}
else
{
setAlpha(255);
}
draw(getAbsoluteRect());
}
In another c-file:
hotBtn.Setup(true, !waterContainerDisplay_Hot.GetWaterContainer()->IsActive(),
waterContainerDisplay_Hot.GetWaterContainer()->GetIconID(),
waterContainerDisplay_Hot.GetWaterContainer()->GetName() );
Do you have enough code like this?
Also, when I use your code, I cannot print the string any lower than the icon of the button.
Thank you for your help!