2021-06-06 04:51 AM
I installed TouchGFX Designer in both CubeIDE and CubeMX.
How do I actually start it?
2021-06-06 05:08 AM
I just discovered that TouchGFX Designer is Windows only, while the rest of the ST development ecosystem is multiplatform.
Please, consider mentioning this issue more prominently.
2021-06-06 11:38 AM
I wanted to report that TouchGFX Designer can be used on a Windows 10 guest system, hosted by Ubuntu with KVM. You can just pass the USB to the guest system and program the board from there.