cancel
Showing results for 
Search instead for 
Did you mean: 

How to display 14-bit gray pixel data through LTDC module.

SPark.28
Associate II

I'm testing the 14-bit (or 16-bit) output from ADC to display using LTDC module.

There is L8 mode among LTDC input types, so I checked the ADC output by normalizing it to 8-bit.

But, what i really need is 14-bit (or 16-bit) gray output.

I want to know how to set LTDC to output 14-bit gray data.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

LTDC can send max 24bit data , if you have special display you can show what you mean , but normal gray scale is only 8bit .