cancel
Showing results for 
Search instead for 
Did you mean: 

How to design a multi-language keyboard on TouchGFX using Unicode characters numbers?

MiladChalipa
Senior

Hi everyone

I am looking for a solution about designing a multi-language keyboard on TouchGFX using Unicode characters numbers which means when the specific language for GUI selected, The letters of keyboard changes according to the language and when the specific button ("a" for instance) has pressed, the corresponding Unicode number for that character send to backend program and the letter correspond to that number typed in text area wildcard.

for example : when the language is on EN, the "a" button emit number "61" and print the letter in text area.

As I searched before, This is the most simple and fast way (with minimal coding) to do, If there is another solution I will be appreciated for your help.

0 REPLIES 0