2017-11-16 12:29 AM
I'm trying to setup some gui windows using STemWin. It would be very helpful if I could compile some simulations to run on a PC (I suppose Windows, Linux is out of the question?).
I have seen that in the STM32Cube_FW_F4_V1.17.0/Middlewares/ST/ST/STemWin/Simulation/ directory there are GUISim.lib, SimulationMinGW.res and WinMain.c files, but I have not found documentation on how I should use them (note that I don't know Windows as well as I know Linux). The STemWin Reference Manual has a chapter on simulation but does not mention these files.Where can I find a step-by-step guide to compile an STemWin simulation running on PC?
Where can I find some example that I can start from? Where can I find examples for both MSVC++ and MINGW (I suppose that MINGW is supported given the name of the foo file SimulationMinGW.res) best regards Max#stemwin #stm32f4 #simulation #mingw2017-11-16 1:26 AM
Hello,
Have you looked to thisApplication Note
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fst-web-ui%2Fstatic%2Factive%2Fjp%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2FDM000896pdf
?
I'd highly recommend you to have a look to STemWin examples under STM32Cube F4 package as: STM32Cube_FW_F4_V1.0\Projects\STM32469I_EVAL\Applications\STemWin.Best Regards
Imen
2017-11-16 3:52 AM
I read the AN4323 application note, but no reference to simulation.
I have taken a look at the examples you mentioned but I have not found out how to compile these examples and have them run in a simulation on PC.
then, how to use the files GUISim.lib, SimulationMinGW.res and WinMain.c?
best regards
Max
2018-05-04 7:56 PM
Have you found the way to build simulation? if you check STM32Cube_FW_F7_V1.xx.x\Projects\WIN32\STemWin_Simulation, there is a Visual Studio file which you can open and configuration is needed in order for you to compile it.