cancel
Showing results for 
Search instead for 
Did you mean: 

How do resolve the Bus fault error causing to hard fault interrupt? it is happening when using the DCMI with DMA in STM32H730 IDE: STM32 CubeIDE and for more details please check the attached USB_CAM pdf particularly when i am using the DCMI with DMA

Skuma.12
Associate II

0693W00000ANpHYQA1.png0693W00000ANp9eQAD.png0693W00000ANp9UQAT.png0693W00000ANp91QAD.png

5 REPLIES 5
RWard.2
Associate

Did you check Configurable Fault Status Registers (CFSR) - 0xE000ED28? You should first check the registries to see a summary of the fault for better troubleshooting. If no, try UsageFault Status Register (UFSR) - 0xE000ED2A. If you want I can help you in a week after I return to my property in Larnaca

Skuma.12
Associate II

you can find the CFSR and HSFR register status in attached pictures

Skuma.12
Associate II

Is there any one to help me on this, want to solve above problem as soon as possible

Thanks in advance.

Skuma.12
Associate II

0693W00000ANp9eQAD.png0693W00000ANp9UQAT.png

Please see the below Pictures and try to help me on this as soon as possible0693W00000ANp9eQAD.png0693W00000ANp9UQAT.png