2020-09-24 11:59 PM
I want to display a long "wchar_t" type text in a textArea.
Here is my code.
void seasoningDisplay::setSeasoningText(const wchar_t* input)
{
touchgfx::Unicode::UnicodeChar tmpfmt[200];
touchgfx::Unicode::strncpy(tmpfmt, (const char*)input, 200);
Unicode::snprintf(seasoningTextBuffer, SEASONINGTEXT_SIZE, "%s", tmpfmt);
seasoningText.resizeToCurrentText();
seasoningText.invalidate();
}I know it is not correct, please tell me how to realize it.
2020-09-28 7:49 AM
What\re you putting into `input`? UnicodeChar is 16-bit unsigned int, so just make sure your conversion matches that.
2020-09-29 2:00 AM
Yes. I use this function like:
setSeasoningText(L"这是中文");I used to think I need to use "touchgfx:: Unicode:: strncpy (tmpfmt, (const char *) input, 200) " to break through the textarea display size (63). It is my foolly.
Now I write the function like this:
void seasoningDisplay::setSeasoningText(const char* input)
{
setlocale(LC_ALL, "chs");
wchar_t *m_wchar = NULL;
int len = mbstowcs(m_wchar, input, 100) + 1;
m_wchar = new wchar_t[len];
mbstowcs(m_wchar, (const char*)input, 100);
Unicode::snprintf(seasoningTextBuffer, SEASONINGTEXT_SIZE, "%s", m_wchar);
seasoningText.resizeToCurrentText();
seasoningText.invalidate();
memset(m_wchar,0, len);
delete m_wchar;
setlocale(LC_ALL, "C");
}By the way, It failed only in real board (compiled by keil). I works in PC simulator.
It just work when I use the char* like"12345". When I use the chinese character. I failed due to the exception of "mbstowcs".
So, how to setup keil make it work?