2019-07-16 11:46 AM
Hello! Has anyone ever already connected the physical buffer of the STM32L4R9 discovery board on the external PSRAM (with or without using GFXMMU)? All STM32 Cube examples are using a buffer in internal RAM...
When I put the buffer in PSRAM, the rendering on LCD is wrong: some white lines appear and sometimes all the content is wrong.
Actually, I have some LTDC FIFO underrun interrupts. I have follow advices of application note DM00287603.pdf (chapter LTDC required bandwidth) without success.
2019-10-11 02:12 AM
Hello David,
I currently try to do the same without satisfaction.
Did you manage to put the physical area of GFXMMU to PSRAM ?
Thanks
Simon