2023-02-20 10:10 AM
I connected JP1 part to 3.3V pin, Gnd to Gnd pin, Mosı, Mıso, CS and Clk pin to CS,Mosı,mıso, sck pins of the microcontroller in CN7 with the help of jumpers.
Bu't I dont know where my DCMI connection(CN4) and shutter, flash connection get interacted with nucle 144 board via using only jumpers. My aim is to get live view from the camera to control my output with buzzer or something else. All connecitons I checked from the internet are done with a display camare done with FFC Cable but ı am trying to connect the module to microcontroller via only using jumper cables
thanks
Solved! Go to Solution.
2023-02-20 11:22 AM
Does the NUCLEO board even expose the DCMI pins you'd need?
Perhaps check the schematics of the EVAL or DISCO boards with support for the camera, and see what the pin combinations are there.
2023-02-20 11:22 AM
Does the NUCLEO board even expose the DCMI pins you'd need?
Perhaps check the schematics of the EVAL or DISCO boards with support for the camera, and see what the pin combinations are there.
2023-02-20 11:46 AM
Okay. Thank you.