cancel
Showing results for 
Search instead for 
Did you mean: 

How can I connect my B CAMS OMW module to STM32H7A3ZIQ Nucleo 144 board?

agala.1
Associate II

I connected JP1 part to 3.3V pin, Gnd to Gnd pin, Mosı, Mıso, CS and Clk pin to CS,Mosı,mıso, sck pins of the microcontroller in CN7 with the help of jumpers.

Bu't I dont know where my DCMI connection(CN4) and shutter, flash connection get interacted with nucle 144 board via using only jumpers. My aim is to get live view from the camera to control my output with buzzer or something else. All connecitons I checked from the internet are done with a display camare done with FFC Cable but ı am trying to connect the module to microcontroller via only using jumper cables

thanks

1 ACCEPTED SOLUTION

Accepted Solutions

Does the NUCLEO board even expose the DCMI pins you'd need?

Perhaps check the schematics of the EVAL or DISCO boards with support for the camera, and see what the pin combinations are there.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

Does the NUCLEO board even expose the DCMI pins you'd need?

Perhaps check the schematics of the EVAL or DISCO boards with support for the camera, and see what the pin combinations are there.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
agala.1
Associate II

Okay. Thank you.