2021-08-06 11:19 AM
2021-08-06 12:28 PM
Presumably you mean the STM32F429I-DISC board?
The manual should indicate all of the free/available pins on the board.
Likely to be very limited as LCD+SDRAM eat most of the pins.
2021-08-06 12:33 PM
Yes on STM32F429I DISC board can we interface please kindly give me information as iam new to stm32
2021-08-06 12:58 PM
I'm not sure how interfacing a 4x4 key pad on an STM32 differs materially from doing it on any other MCU from the last 3 decades.
You presumably want to find 4 output pins and 4 input pins in the simplest implementation.
Or drive the outputs via a 2-to-4 decoder type IC
Seem to recall there being chips these days that would drive 8-led and offer and bunch or inputs/outputs.
Also perhaps an I2C Bus Expander type chip?
Going to START with you pulling the MANUAL for the board and identifying the free/available pins to do things with..
2021-08-06 1:05 PM
The TM1638 is what I was thinking of
DIY KIT TM1638 Digital LED Display 3-Wire 16 Keys 8 Bits Keyboard 8-Bit Digital Tube Board Scan And KEY LED Module For Arduino
https://www.aliexpress.com/item/32838376871.html