HardFault when upgrading TouchGFX 4.9.3 to 4.10.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-27 7:30 PM
Hi ST Community,
​
I've ported touchgfx on my custom board, and it runs successfully. The hardware and software configuration is as follows,
​
HW configuration
CPU -> STM32L4R9 family
SW configuration
IAR 8.30
TouchGFX Designer 4.9.3
​
Now, I'm trying to upgrade TouchGFX Designer to 4.10.0, I do the following steps,
- open the project in TouchGFX Designer 4.10.0, and choose "Yes" to upgrade (TouchGFX Designer 4.10.0 will download something, seems like touchgfx core)
- run simulator successfully
- generate code in TouchGFX Designer 4.10.0
- open the project in IAR, and rebuild the project
- download the image to the custom board, and it crash.
I backup the call stack when crashing as follows. It crash when touchgfx_generic_init() -> FrontendHeap::getInstance(); is called.
HardFault_Handler
<Exception frame>
[_ZN8touchgfx6Screen4drawEv + 0x23]
[_ZN8touchgfx11ApplicationC1Ev + 0x61]
touchgfx::MVPApplication::MVPApplication()
touchgfx::MVPApplication::subobject MVPApplication()
FrontendApplicationBase::FrontendApplicationBase(class Model &, class FrontendHeap &)
FrontendApplicationBase::subobject FrontendApplicationBase(class Model &, class FrontendHeap &)
FrontendApplication::FrontendApplication(class Model &, class FrontendHeap &)
FrontendHeap::FrontendHeap()
FrontendHeap::getInstance()
class touchgfx::HAL & touchgfx::touchgfx_generic_init<STM32HAL_SPI>(class touchgfx::DMA_Interface &, class touchgfx::LCD &, class touchgfx::TouchController &, signed short, signed short, unsigned short *, unsigned int, unsigned int)
touchgfx::touchgfx_init()
GRAPHICS_Init()
I have no idea so far, can anyone help to look into the issue? Thanks!
Solved! Go to Solution.
- Labels:
-
TouchGFX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-27 8:41 PM
When the library became exclusive to ST chips, they added a check to make sure it's running on ST hardware which uses ST's CRC peripheral. This means you need to enable the clock for the CRC peripheral before it tries to use it. I don't know when exactly touchgfx checks for this so can't tell if this is your issue based on the call stack but try adding
__HAL_RCC_CRC_CLK_ENABLE();
sometime before initializing touchgfx to see if that fixes it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-27 8:41 PM
When the library became exclusive to ST chips, they added a check to make sure it's running on ST hardware which uses ST's CRC peripheral. This means you need to enable the clock for the CRC peripheral before it tries to use it. I don't know when exactly touchgfx checks for this so can't tell if this is your issue based on the call stack but try adding
__HAL_RCC_CRC_CLK_ENABLE();
sometime before initializing touchgfx to see if that fixes it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-27 10:26 PM
@Community member​
Thanks for your quick response.
Yes, Indeed. As you said, the crash is due to CRC peripheral not enabled. I've verified it works. Thank you!
Hope ST can provide a upgrade guide with TouchGFX Designer release.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-04-02 5:19 AM
Hi @L4Y​,
The fact that you couldn't find this information is good input to us in some way. Sorry for the trouble. And thanks to @Community member​ for stepping in!
https://touchgfx.zendesk.com/hc/en-us/articles/207507415-Known-Issues
Best regards,
Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-03 3:25 AM
Still true and working solution in 2022 ! Many thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-30 8:01 AM
Sorry, but now in 2024 this solution doesn't work for me.
I'm trying to develop a custom board touchgfx project with TouchGfx 4.23.0, STM32CubeIDE 1.14.1, STM32CubeMX 6.10.0. MCU is STM32WL5MOCH (Cortex M4).
I've generated the project with CubeMX itself.
MX_CRC_Init() (with __HAL_RCC_CRC_CLK_ENABLE();) is called before MX_TouchGFX_Init().
I have a systematic Hard Fault here:
In _ZN8touchgfx6Screen4drawEV, during instruction str r1, [sp, #0]:
Here are the registers:
What could be the problem?
Thank you