cancel
Showing results for 
Search instead for 
Did you mean: 

GFX designer invalid patch STM32F7 disco

Vojtěch
Associate II

Hello,

I created a project in Touch GFX designer. Then I open in STM32cubeIDE, but I get a warning:

Description   Resource   Path   Location   Type

Invalid project path: Include path not found (C:\TouchGFXProjects\MyApplication_1\Middlewares\Third_Party\FreeRTOS\Source\CMSIS_RTOS).   STM32F746G_DISCO      pathentry   Path Entry Problem

thank you for answer

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Yoann KLEIN
ST Employee

Hello @Vojt?ch​ ,

Did you enable FreeRTOS in CubeMX and generated code ?

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX
Vojtěch
Associate II

My project was generated by Touch gfx designer. Then I ran the code in stm32cubeIDE.

Yoann KLEIN
ST Employee

I cannot reproduce your error, which version of TouchGFX are you using ?

Yoann KLEIN
ST Software Developer | TouchGFX
Vojtěch
Associate II

Touch GFX 4.20.0

Yoann KLEIN
ST Employee

Could you please generate code in CubeMX for this project ?

Yoann KLEIN
ST Software Developer | TouchGFX
Karl Yamashita
Principal

Somehow your path to /Third_Party/FreeRTOS/Source/CMSIS_RTOS doesn't seem right if you had TouchGFX generate the code.

When I create a project from TouchGFX, import into STM32CubeIDE and build, I see /Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source