cancel
Showing results for 
Search instead for 
Did you mean: 

Designer: When import fails unexpectedly - it leaves the project in invalid state.

HTD
Senior III

The problem appeared when I deleted a custom container that contained a specific font. I also deleted the typography. Then for a test purpose, I imported the custom container again. I got an error, that my font file is being open, so the import process cannot write it.

The import failed leaving some files imported, and some not imported. I had to manually delete imported files and restart TouchGFX to be able to import the custom container.

What IMO should happen - if the import fails, it should roll back the changes, or... maybe ignore the error and continue with the rest of the files. When unexpected error occurs - the best solution would be to display a dialog like this:

An error occurred while importing the custom container

Proceed with:

  1. Roll back the changes (remove imported files)
  2. Ignore the error and continue (some files may be missing)

 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Hello @HTD ,

Sorry for the inconvenience, we will definitely consider this issue for improving.
Thanks for the report and suggesting.

Mohammad MORADI
ST Software Developer | TouchGFX