2017-07-28 9:16 PM
hi everybody,
i have worked tft projects through normal gpio pins, ie a parallel bus + some control lines, since now.
i saw the FSMC in the STM32F407 micro controller which can do that for me.
i don't know the difference between these tow method.
thanks, Rasool
#gpio #tft #fsmc #lcd #stm322017-07-28 9:42 PM
The address, data and control signals are sequenced in hardware rather than bit-banging. Review the timing diagrams, and signal parameters described in the Reference Manual. It's an external memory bus, similar to those used with micro-controllers for several decades.
2017-07-29 6:10 AM
if i think true the cpu load decreases.
is the 'time to display' and in fact transfer time from mcu to lcd controller decrease?
what about for power consumption?
2017-07-29 8:46 AM
>>what about for power consumption?
Well the bus transaction will be more efficient. But you could also saturate the bus at a much higher rate. Power consumption will depend on the duty cycle of your use case.
Measure, then compare and contrast.