2019-12-30 10:33 PM
While using touchGFX, which font files should be used for the following languages
1.German,
2.english,
3.french,
4.spanish,
5.italian,
6.portuguese,
7.swedish,
8.russian,
9.czesh,
10.polish,
11.chinese,
12.japanese,
13.korean,
14.turkish
For each font file what would be the memory required?
Solved! Go to Solution.
2020-01-08 04:22 AM
I can't answer that. It's up to you which font you want to use - You need to investigate if that font has the unicodes that suit your needs for some language. Memory requirements (flash) depend on the size defined by the typography you define in TouchGFX and the quality of the font.
/Martin
2020-01-08 04:22 AM
I can't answer that. It's up to you which font you want to use - You need to investigate if that font has the unicodes that suit your needs for some language. Memory requirements (flash) depend on the size defined by the typography you define in TouchGFX and the quality of the font.
/Martin