cancel
Showing results for 
Search instead for 
Did you mean: 

Fast switch between selected Languages in TouchGFX Designer

GS1
Senior III

I am creating a user interface in German and English language. In order to compare the german and english presentation it is quite often necessary to switch between the selected language. This is currently only possible by several steps:

  • select the "Config" button in the left side menu
  • then change the Selected Language in the Pulldown option
  • then change back to the Canvas menu

It would be a great help to have a more direct access to the language change function via a separate menu entry, which is always accessible in the canvas presentation or maybe even a keyboard shortcut.

If there is already something like that available, then I am thankful for a hint.

BR GS

1 REPLY 1
Osman SOYKURT
ST Employee

Hello GS@S,

This isn't possible for now unfortunately. But the idea is great, thank you for this suggestion :)

This is definitely a feature that we can add in the future. I'll let you know when I'll have more information about it.

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX