cancel
Showing results for 
Search instead for 
Did you mean: 

External Memory Error when flashing Nucleo-575ZI-Q + GFX02Z1 via TouchGFX or CubeIDE

Neyus
Associate III

Hello,

this error really drives me crazy. When trying to flash the programm from the ToughGFX App or CubeIDE the external Memory can't be erased. I use the recommended CubeMXVersion of 6.14 and have the latest CubeProgrammer and CubeIDE with STM32Cube FW_U5 V1.7.0. The whole ToughGFX log is attached. Thanks in advance!

These are the following errors that are occurring:

TouchGFX:

Erasing memory corresponding to sector 0:
Erasing external memory sector 0
Error: failed to erase memory

gcc/include/flash_sections_int_ext.mk:5: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 1
../gcc/Makefile:52: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed

 

CubeIDE:

Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

\STM32CubeIDE\\Debug\\STM32U575ZI-NUCLEO-AZ2.elf

Error message from debugger back end:

Error finishing flash operation

Error finishing flash operation

 

13 REPLIES 13

Do you mean the TouchGFX project? I’ve only tested the board combination using either a blank screen or a single button—just the "Board Selector" and "Blank" options. I haven’t done anything else beyond that.

LouisB
ST Employee

I dont see what it can be, but If you were never able in the past to flash the external memory, I suspect that you have a faulty board. If you have a other board available you can try to be sure.

 

BR,

Louis BOUDO
ST Software Engineer | TouchGFX
LouisB
ST Employee

@Neyus, is the screen connected when you try to erase memory ?

Louis BOUDO
ST Software Engineer | TouchGFX

@LouisB yes the screen is in its dedicated socket on the nucleo STM Board when trying to erase the memory or flash it with TouchGFX. I do not have a second screen available to test if its a faulty board.