2021-04-16 01:34 AM
Hi,
When I was creating a UI template before format my laptop, it was ok. But now, When I was trying to create an ui temp, I got the error like object reference not set to an instance of an object. What is the problem?
2021-04-16 06:12 AM
Hi,
Could you share a screenshot of your error ? What does you json look like ?
There is an issue at the moment with the tool and the latest versions of TouchGFX Environement, so make sure you are using TouchGFX Environment 4.14 and below to create application templates or UI templates.
We hope to release the fix very soon.
/Romain
2021-04-16 06:22 AM
Hi,
I was creating the UI template with 4.14 version and it was okey. I had a problem with my laptop and format it. But now I got the "object reference not set to an instance of an object" error. I used an example of TouchGFX designer to make sure the error wasn't caused by my project and I got the same error.