2019-02-28 10:30 AM
Hello,
I used STM32F769I-EVAL board as a design reference for custom board. However, I could not achieve correct operation of MB1166 LCD board
which is connected via DSI. It works well on the evaluation board.
When MCU tryies to display a picture, screen fickers with coloured lines and stays white.
Theres some hardware problem which I cannot figure out. Im attaching custom board schematics of DSI peripheral. STM32F769BIT6 MCU is used.
Any help to debug such issue would be apriciated.
2019-02-28 5:43 PM
Schematics looks fine at first glance, did you double check layout for footprints missmatch and doubled check the differential pairs for proper routing?
2019-02-28 9:55 PM
Dear Du,
footprints are correct. I figured that DSI routing could have been a problem on my first PCB design. So this time I designed around the DSI. My approach was to reduce length of DSI route as short as possible while maintaining DSI_CK, DSI_D0 and DSI_D1 lengths as equal as possible.
Im attaching PCB routing of DSI connection and DSI net lengths.
2019-02-28 10:17 PM
2019-03-01 2:42 AM
Code was not changed. I upload the same hex file through STM32 ST-LINK Utility. It works on evaluation board and does not on custom board.
Disconnected lcd screens from both boards and checked if signals and voltage levels of LCD connector pins are the same. It was ok and pins were not mixed. Only difference was that at on the discovery boards pin LCD connections 37 pin was high. However, on LCD MB1166 board this pin was disconnected so it should not be the source of the issue.
Checked crystal oscilators frequency - 25 MHz same as on evaluation board. I captured signals of DSI channels from custom board. Cold you check if it looks ok, because D1 signals look suspicious.
Im using new MCU. Does it need any specific configuration before uploading the code to flash?
2019-03-01 11:13 PM
Can you capture the first 500mS of activity on the eval board and then the custom board and compare the two oscope shots to each other?
I don't have the datasheet for the LCD board, does that LCD use D1 channel?
Are you using the same part numbers for the crystals and any other clock related sources?
2019-03-02 3:59 AM
LCD boards datasheet: https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/10/0d/a5/a2/7e/b9/4c/ca/DM00321394/files/DM00321394.pdf/jcr:content/translations/en.DM00321394.pdf
Yes, it should use D1 channel. I will capture CLK, D0,D1 and TE signals in few upcoming days.
Crystal oscillators part numbers are different, however parameters are the same. I double checked amplitude and frequency with the oscilloscope of both boards.
2019-03-02 6:39 AM
Perhaps have an ST FAE review the PCB and trace layout/lengths, circuit performance likely to be critical at these speeds.
2019-03-05 2:45 AM
Dear Du,
I attached eval board and custom boards DSI signals. Captured oscilograms are from MB1166 LCD side.
Data signals seems to be fine.
Im uploading hex file from "STM32F769I_EVAL\Applications\Display\LCD_DSI_ImagesSlider" example. It uses DSI LCD screen and external QSPI flash which is placed on my custom board. Hex successfully flashes. I also tried applications which does not used external flash. The issue remains.
Do you have any other suggestions? Ill try to sample and compare more signals from LCD side.
2019-03-05 2:47 AM
Dear Clive Two.Zero,
I will try to contact them through the supplier of the evaluation board.