2023-03-13 12:56 AM
Hi, I created a list and I need set visible image when element of the list is clicked
But problem is that others drawables does not unselected when pressed one of the list elements. When I click on list element I call this function
void AddZone::ZoneSelected()
{
SelectedZone.setVisible(true);
}
How to unselect others when one of them is pressed? (I can't use radio button because I need scaleable image)
2023-03-13 2:33 AM
Hi,
Could you give a bit more context on how your code works ? How is your list implemented ? Are you using a list layout widget or is it through another implementation or user code ?
What are those selectedZone that you set visible ? I guess it is a kind of background image you turn visible according to your screenshot ? Could you not just implement a function that sets all of those background images invisible before setting the correct one to visible ? (terrible coding I know :grinning_face_with_sweat: but we need more context on your side anyway to give a better implementation)
/Romain
2023-03-13 3:24 AM
Yes Im using listlayout .SelectedZone is scalable image which becomes visible when I click. First of all when I click this button:
it calls function below which creates list elements:
void InputOutpuConfigurationView::AddNewZone()
{
uint8_t zoneadd = addzone;
FansExpandss.setVisible(false);
FansExpand.setVisible(false);
Fans.setVisible(false);
fans.setVisible(false);
DeleteZone.setVisible(true);
uint8_t SavedIdx = presenter->getZoneVal();
if(SavedIdx != addzone-1)
addzone = SavedIdx+1;
if(addzone<11)
{
presenter->SaveClickedZone(addzone);
presenter->ZoneVal(addzone);
ZoneClicked(addzone);
selectedzone.setX((86*(addzone))+zonescroll.getScrolledX());
Unicode::snprintf(zoneheadlineBuffer, ZONEHEADLINE_SIZE, "%s - %d",TypedText(T_ZONE).getText(),addzone);
presenter->SaveZoneHeadline(zoneheadlineBuffer,addzone,0);
for (uint8_t i = 0; i < addzone; ++i)
{
zonelist.remove(ZoneElements[i]);
}
zoneadd = presenter->getZoneVal()+1;
while(zoneadd > 0)
{
zonelist.setHeight(0);
ZoneElements[zoneadd-1].setupListElement(presenter->getHeadlineOfZone(zoneadd),zoneadd,16,156,241,zoneadd,presenter->getModified(zoneadd));
zoneadd--;
}
if(zoneadd == 0)
{
addzone = presenter->getZoneVal();
for (uint8_t i = 0; i < addzone; ++i)
{
ZoneElements[i].setAction(listElementClickedCallback);
zonelist.add(ZoneElements[i]);
}
}
}
if(addzone>0 && addzone<11)
addzone++;
}
"setupListElement" sets name, index, color..
void AddZone::setupListElement(Unicode::UnicodeChar* txt,uint8_t add,colortype R,colortype G,colortype B, int _index,int8_t modified)
{
index = _index;
Unicode::snprintf(zonetxtBuffer, ZONETXT_SIZE, "%s",txt);
zonetxtBuffer[ZONETXT_SIZE-1] = '\0';
zonetxt.setColor(touchgfx::Color::getColorFromRGB(R, G, B));
zonetxt.resizeToCurrentTextWithAlignment();
invalidate();
}