Displaying Data to TouchGFX UI using wildcards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-06 02:34 AM
Hi Guys
I am a noobie and I am just starting out with TouchGFX. I have designed a 7 screen gui which cycles between screens (1-7 in that order which cylces indefinitely) and I have a text area which I want to populate with real-time data. This is only on screen 4 and 6 and I have defined the wildcards in the designer as follows:
I have generated the code using TouchGFX 4.23.2 and then I open the IOC file in CubeMX where I add ADC initialization as well as two tasks and two semaphores. One to update screen4 and one to update screen6, I then generate the code in MX and then click on "Open Project" to import it into CubeIDE.
I do not know where to take it from here. Essentially I want to read an ADC voltage (polling) in the two tasks I have created, then from there update screen4 and screen6 wildcards when the screen is loaded.
Here is my main.c:
I have tried to follow this video: https://www.youtube.com/watch?v=EbWOv_0Lp-U&t=241s, however when I adapt it to 7 screens and 2 semaphores and tasks, I upload the code to my STM32F429i-DISC1 and I just observe a white screen, however when I upload the code without having made any modifications in STMCubeIDE as seen in the video, I see the desired gui implemented with the exception of the real time data being displayed on screen 4 and 6.
Any help would be appreciated thanks.
Solved! Go to Solution.
- Labels:
-
TouchGFX
-
TouchGFX Designer
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-06 05:45 AM
This is The code which I found works in case anyone was wondering.
void Screen4View::UpdateVoltage(float value)
{
Unicode::snprintfFloat(textAreaVoltageBuffer,sizeof(textAreaVoltageBuffer), "%.2f V", value);
textAreaVoltage.invalidate();
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-06 03:54 AM
Ok, so I have worked on it longer and I have gotten to this point:
I call a function in my Screen6View.cpp which I want to update the wildcard value in the gui.
This is how my code looks:
#include <gui/screen6_screen/Screen6View.hpp>
#include "string.h"
Screen6View::Screen6View()
{
}
void Screen6View::setupScreen()
{
Screen6ViewBase::setupScreen();
}
void Screen6View::tearDownScreen()
{
Screen6ViewBase::tearDownScreen();
}
void Screen6View::UpdateCurrent(float value)
{
Unicode::UnicodeChar buffer[6];
Unicode::snprintfFloat(buffer,sizeof(buffer), "%.2f", 3.15345);
textAreaCurrent.setWildcard(buffer);
textAreaCurrent.invalidate();
}
When I debug my board, I can see that I am entering the UpdateCurrent function. I set the Initial value of the wildcard to be -1 and ass soon as I call my UpdateCurrent function the wildcard updates to the fallback character of the wildcard which I set to be '-' in touchGFX.
When I inspect the contents of buffer during runtime I see the following:
buffer[0] = 51
buffer[1] = 46
buffer[2] = 49
buffer[3] = 53
buffer[4] = 0
buffer[5] = 42405
I know buffer[0]-buffer[4] is supposed to represent 3.15 with null termination.
I just don't know why the embedded gui is updating the wildcard with the fallback character '-'.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-06 05:45 AM
This is The code which I found works in case anyone was wondering.
void Screen4View::UpdateVoltage(float value)
{
Unicode::snprintfFloat(textAreaVoltageBuffer,sizeof(textAreaVoltageBuffer), "%.2f V", value);
textAreaVoltage.invalidate();
}