cancel
Showing results for 
Search instead for 
Did you mean: 

Dear Experts, I am new in using STM32H735-DK board. tried to download clock example in developement board. Download succeed but example not working. Two LEDS,LD1 & LD2 continues ON and display Blank. when i press RST button display just blink only.

Dharmesh
Associate II

STMicroelectronics ST-LINK GDB server. Version 5.9.1

Copyright (c) 2021, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.8.0          

   -------------------------------------------------------------------

ST-LINK SN : 001F00303438510734313939

ST-LINK FW : V3J8M3

Board    : STM32H735G-DK

Voltage   : 3.29V

SWD freq  : 24000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x483

Revision ID : Rev Z

Device name : STM32H72x/STM32H73x

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x92

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a21916.srec

 File     : ST-LINK_GDB_server_a21916.srec

 Size     : 386412 Bytes

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Erasing internal memory sector 0

Erasing memory corresponding to segment 1:

Erasing external memory sectors [0 3]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:03.765

Verifying ...

Download verified successfully 

Debugger connection lost.

Shutting down...

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee

Hi @Dharmesh​ ,

Based on the readme file of the example STM32CubeH7/Projects/STM32H735G-DK/Examples/RCC/RCC_ClockConfig, the clock source is changed each time you press the USER button.

  • LED1 is toggled with a timing defined by the HAL_Delay() API.
  • LED2 is ON when there is an error.

Is that what you see as behavior?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello Amel,

Thank you for your reply.

Problem was solved when i uninstall STCube IDE,Ver_6.0 and install latest one.But again same thing happening right now. in my Discovery board when i load even simple program of one screen touch gfx,simulation working fine, firmware download succsed but LD1,LD2 continuesly Glow and display black.. When i press RESET button sitution as it is.

I am using below IDE right now,

  1. st-stm32cubeide_1.9.0_12015_20220302_0855_x86_64
  2. TouchGFX-4.19.1

When i tried for debugging i found firmware is not getting out from below loop of core_cm7.h file

sets = (uint32_t)(CCSIDR_SETS(ccsidr));

  do {

   ways = (uint32_t)(CCSIDR_WAYS(ccsidr));

   do {

    SCB->DCISW = (((sets << SCB_DCISW_SET_Pos) & SCB_DCISW_SET_Msk) |

           ((ways << SCB_DCISW_WAY_Pos) & SCB_DCISW_WAY_Msk) );

    #if defined ( __CC_ARM )

     __schedule_barrier();

    #endif

   } while (ways-- != 0U);

  } while(sets-- != 0U);

  __DSB();

waiting for your valueable feedback. Thank you.

Hi @Dharmesh​,

TouchGFX is not my area of expertise. May be @Romain DIELEMAN​  can help you at this level.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.