cancel
Showing results for 
Search instead for 
Did you mean: 

Customized circle progress

KNara.2
Associate III

Hi,

I'm looking at customising the circle progress.

KNara2_0-1704292274992.png

I was able to add this as the background image 

KNara2_1-1704292433716.png

and added a single dot as the image to rotate.

Any idea on how to rotate the dots and make it disappear?

 

1 ACCEPTED SOLUTION

Accepted Solutions

You are very welcome.

I think having two different circle progresses would be easier to handle. However, if you prefer to do it in code, you can use these two functions:

// To change the background circleProgress.setBackground(touchgfx::Bitmap( /* Bitmap ID of the background */ )); // To change the progress image circleProgressPainter.setBitmap(touchgfx::Bitmap( /* Bitmap ID of the progress image */));

Keep in mind that you need to change the attributes of the progress to show it properly. 
You can read more circle progress here .

 

I hope this helps

Mohammad MORADI
ST Software Developer | TouchGFX

View solution in original post

7 REPLIES 7

Hello @KNara.2 ,

There is a Progress Indicator example on TouchGFX which contains a circular indicator similar to the one you desire.

Progress Indicator ExampleProgress Indicator Example

 

Please consider checking it for inspiration and if you still need help, don't hesitate to ask.

Mohammad MORADI
ST Software Developer | TouchGFX
KNara.2
Associate III

@Mohammad MORADI ESFAHANIASL 

Thanks that was useful.

I'm looking at implementing a circle progress where in at the first iteration I have one background image and one progress image, in the next iteration I want to swap these two images.

Any leads on how this can be achieved?

Should I use 2 circle progress and call them in loop one after another?
Is there a feature called reverse for circle progress, just like the animated images have?

Please guide.

Thanks.

You are very welcome.

I think having two different circle progresses would be easier to handle. However, if you prefer to do it in code, you can use these two functions:

// To change the background circleProgress.setBackground(touchgfx::Bitmap( /* Bitmap ID of the background */ )); // To change the progress image circleProgressPainter.setBitmap(touchgfx::Bitmap( /* Bitmap ID of the progress image */));

Keep in mind that you need to change the attributes of the progress to show it properly. 
You can read more circle progress here .

 

I hope this helps

Mohammad MORADI
ST Software Developer | TouchGFX

Thanks for all the guidance @Mohammad MORADI ESFAHANIASL 

I used touchgfx_printf() calls (needs <touchgfx/Utils.hpp>) and was able to debug in simulator.

Thanks again.

Hi @Mohammad MORADI ESFAHANIASL 

There is a slight flicker that is seen when the images are swapped.

Any solution for this?

This is how my code looks

void Screen1View::setupScreen()
{
tickCounter = 0;
Screen1ViewBase::setupScreen();

flag = true;
}

void Screen1View::handleTickEvent()
{
     int n;
    tickCounter++;
    updateProgress(tickCounter);
    updateDirection(tickCounter);
    n = circleProgress1.getValue();
 
    if (circleProgressMax-1 == n)
    {
    if(flag)
    {
       circleProgress1.setBackground(touchgfx::Bitmap(BITMAP_FULL_ID));
        circleProgress1Painter.setBitmap(touchgfx::Bitmap(BITMAP_VACANT_ID));
        circleProgress1.invalidate();
        flag = false;
    }
    else
    {
         circleProgress1.setBackground(touchgfx::Bitmap(BITMAP_VACANT_ID));
          circleProgress1Painter.setBitmap(touchgfx::Bitmap(BITMAP_FULL_ID));
          circleProgress1.invalidate();
          flag = true;
    }

I got the fix for flickering issue.

Posting the solution here, in the hope that it might help someone.

I used 

circleProgress1.invalidate();
circleProgress1.invalidateContent();

and the flickering issue/redraw issue is fixed.

Thanks & Regards,

Keerthi.A.N

You're very welcome :D
Glad to hear you got it working

Mohammad MORADI
ST Software Developer | TouchGFX