2024-02-28 03:08 AM
I have generated a new project with Touch GFX Designer where I created a text area and also created a button, to which I have linked an interaction. This interaction will call on a new virtual function which I then plan on integrating with my external project files. I've created my projects .c and .h files in which I'm writing a simple arithmetic calculation. Note that my project files are in C whereas the Touch GFX generated files are in C++, I now want to call the arithmetic function in the model.cpp file and I'm unable to run the simulator on the Designer as it gives me an error.
File Path for Touch GFX generated files -> C:\TouchGFXProjects\MyApplication_2\CM7\TouchGFX\gui\src
Below are the files:
view.cpp
#include <gui/screen1_screen/Screen1View.hpp>
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::ButtonClicked(){
presenter->MathTest(7, 4);
}
void Screen1View::GetResult(uint16_t Result){
char buffer[20]; // Adjust the buffer size as needed
snprintf(buffer, sizeof(buffer), "%u", Result);
Unicode::strncpy(textArea1Buffer, buffer, TEXTAREA1_SIZE);
textArea1.invalidate();
}
view.hpp
#ifndef SCREEN1VIEW_HPP
#define SCREEN1VIEW_HPP
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
#include <cstdio>
class Screen1View : public Screen1ViewBase
{
public:
Screen1View();
virtual ~Screen1View() {}
virtual void setupScreen();
virtual void tearDownScreen();
void ButtonClicked(); //remove virtual
void GetResult(uint16_t Result);
protected:
};
#endif // SCREEN1VIEW_HPP
presenter.cpp
#include <gui/screen1_screen/Screen1View.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
Screen1Presenter::Screen1Presenter(Screen1View& v)
: view(v)
{
}
void Screen1Presenter::activate()
{
}
void Screen1Presenter::deactivate()
{
}
void Screen1Presenter::MathTest(uint16_t x, uint16_t y)
{
model->MathTest(x,y);
}
void Screen1Presenter::GetResult(uint16_t Result)
{
view.GetResult(Result);
}
presenter.hpp
#ifndef SCREEN1PRESENTER_HPP
#define SCREEN1PRESENTER_HPP
#include <gui/model/ModelListener.hpp>
#include <mvp/Presenter.hpp>
using namespace touchgfx;
class Screen1View;
class Screen1Presenter : public touchgfx::Presenter, public ModelListener
{
public:
Screen1Presenter(Screen1View& v);
/**
* The activate function is called automatically when this screen is "switched in"
* (ie. made active). Initialization logic can be placed here.
*/
virtual void activate();
/**
* The deactivate function is called automatically when this screen is "switched out"
* (ie. made inactive). Teardown functionality can be placed here.
*/
virtual void deactivate();
virtual ~Screen1Presenter() {}
virtual void MathTest(uint16_t x, uint16_t y);
// ModelListener callback
virtual void GetResult(uint16_t result);
private:
Screen1Presenter();
Screen1View& view;
};
#endif // SCREEN1PRESENTER_HPP
Model.cpp
#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
#ifndef SIMULATOR
#include "Mytest.h"
#include "stdio.h"
#endif
Model::Model() : modelListener(0)
{
}
void Model::tick()
{
}
uint16_t Model::MathTest(uint16_t x, uint16_t y)
{
#ifdef SIMULATOR
uint16_t Result = MathOp(x,y);///
modelListener->GetResult(Result);
return Result;
#else
return 0.0;
#endif
}
Model.hpp
#ifndef MODEL_HPP
#define MODEL_HPP
#include <cstdint>
class ModelListener;
class Model
{
public:
Model();
void bind(ModelListener* listener)
{
modelListener = listener;
}
void tick();
uint16_t MathTest(uint16_t x, uint16_t y);
protected:
ModelListener* modelListener;
};
#endif // MODEL_HPP
A source file (Mytest.c) -> C:\TouchGFXProjects\MyApplication_2\CM7\Core\Src
Myfile.h -> C:\TouchGFXProjects\MyApplication_2\CM7\Core\Inc
#include "Mytest.h"
uint16_t MathOp(uint16_t x, uint16_t y)
{
return x+y;
}
#ifndef APPLICATION_USER_CORE_MYTEST_H_
#define APPLICATION_USER_CORE_MYTEST_H_
#include <stdint.h> // Include <cstdint> for uint16_t
uint16_t MathOp(uint16_t x, uint16_t y);
#endif /* APPLICATION_USER_CORE_MYTEST_H_ */
The function MathOp was created for the arithmetic calculation which was called in the model.cpp file. Below is the error from the simulator on Touch GFX Designer:
2024-02-28 07:32 AM
Hi @mƎALLEm, I've made the changes as below but I'm getting an error message when I run the simulator:
# Helper macros to convert spaces into question marks and back again
e :=
sp := $(e) $(e)
qs = $(subst ?,$(sp),$1)
sq = $(subst $(sp),?,$1)
# Get name of this Makefile (avoid getting word 0 and a starting space)
makefile_name := $(wordlist 1,1000,$(MAKEFILE_LIST))
# Get path of this Makefile
makefile_path := $(call qs,$(dir $(call sq,$(abspath $(call sq,$(makefile_name))))))
# Get path where the Application is
application_path := $(call qs,$(abspath $(call sq,$(makefile_path)../..)))
.PHONY: clean assets all
ifneq ($(words $(makefile_path))$(words $(MAKEFILE_LIST)),11)
all clean assets:
$(error Spaces not allowed in path)
else
# Add new source file and header file paths
ADDITIONAL_SOURCES := C:/TouchGFXProjects/Test/CM7/Core/Src/Mytest.c
ADDITIONAL_INCLUDE_PATHS := C:/TouchGFXProjects/Test/CM7/Core/Inc
ADDITIONAL_LIBRARY_PATHS :=
ADDITIONAL_LIBRARIES :=
export ADDITIONAL_SOURCES ADDITIONAL_INCLUDE_PATHS ADDITIONAL_LIBRARY_PATHS ADDITIONAL_LIBRARIES
all: $(filter assets,$(MAKECMDGOALS))
all assets: $(filter clean,$(MAKECMDGOALS))
all clean assets:
@$(MAKE) -r -f generated/simulator/gcc/Makefile -s $(MFLAGS) $@ -C "$(application_path)"
endif
Error message:
2024-02-28 07:49 AM
Hello @koderboi22 ,
Your architecture is correct, however, you have defined the include files to be called when the simulator is not running and then you have set to call the function MathOp when the simulator is running. So, if you like to test your code in simulator, you should either remove the Marcos for the simulator or set them both to #ifdef simulator
I hope this helps you, don't hesitate to ask more questions.
2024-02-28 08:02 AM
Indeed, I didn't see this part of code:
#ifndef SIMULATOR
#include "Mytest.h"
#include "stdio.h"
#endif
I focused on the makefile!
2024-02-28 08:35 AM - edited 2024-02-28 08:38 AM
Hi @Mohammad MORADI ESFAHANIASL ,
I have removed them both from the #ifndef SIMULATOR now:
#ifndef SIMULATOR
#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
#else
#include "C:/TouchGFXProjects/Test/CM7/Core/Inc/Mytest.h"
#endif
// Define the constructor for the Model class
Model::Model() : modelListener(0) {}
// Define the tick function for the Model class
void Model::tick() {}
// Define the MathTest function for the Model class
uint16_t Model::MathTest(uint16_t x, uint16_t y) {
#ifndef SIMULATOR
// Include header and call MathOp function when not running in the simulator
return 0;
#else
// When running in the simulator, just return the sum of x and y
uint16_t Result = MathOp(x, y);
modelListener->GetResult(Result);
return Result;
#endif
}
If not, can you please guide how to fix this.
Furthermore, I'm still receiving the same error as well.
2024-02-28 08:38 AM - edited 2024-02-28 08:42 AM
No.
Since you are using the simulator you need to define the flag SIMULATOR:
Replace:
#ifndef SIMULATOR
by
#ifdef SIMULATOR
So you need to remove 'n' from #ifndef
Or simply remove this definition.
2024-02-28 08:44 AM
I've done this however when I now build the code it says, that there is an undefined reference to the MathOp function.
2024-02-28 08:49 AM - edited 2024-02-28 08:52 AM
You need to add Mytest.c file to your project. To my knowledge in the Makefile under simulator\gcc:
ADDITIONAL_SOURCES := ../CM7/Core/Src/Mytest.c
2024-02-28 08:51 AM
So I've made both the changes as you mentioned however still I'm receiving the error, if there is a way to set up a meeting of some kind it'll be great help.
2024-02-28 08:55 AM - edited 2024-02-28 09:05 AM
Unfortunately, no meeting is possible.
If you can attach your project so TouchGFX experts can help you.
If not possible, as said previously, you need to contact your local FAE for an efficient assistance.
2024-02-28 05:07 PM
@koderboi22 If you wish an experienced programmer to look at your code, review and so on - this is available here and here.