cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX + STEmWin + Atollic Integration ETA

Richard Lowe
Senior III
Posted on May 28, 2018 at 17:56

Project generation in CubeMX is great. Atollic now that it is free is great. STEmWin is.... ok. 

I'd like to generate STemWin based projects with CubeMX while using the Atollic IDE. 

As some of you might know, when you ENABLE GRAPHICS in the Pinout,  TrueStudio as the IDE to generate the project for is not available in the project output.

Wondering if anyone at ST has an ETA when TrueStudio / Atollic will be supported?0690X0000060BP6QAM.png

#stemwin #atollic-truestudio #cubemx
1 ACCEPTED SOLUTION

Accepted Solutions
Richard Lowe
Senior III
Posted on June 07, 2018 at 10:12

As of today, CubeMX 4.26.0 now supports TrueSTUDIO with graphics. 

View solution in original post

5 REPLIES 5
Posted on May 28, 2018 at 23:13

What is it ETA?

Posted on May 29, 2018 at 00:57

>>Wondering if anyone at ST has an ETA when TrueStudio / Atollic will be supported?

2019Q4 ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 29, 2018 at 00:58

Estimated Time of Arrival - Delivery date of product

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Richard Lowe
Senior III
Posted on June 07, 2018 at 10:12

As of today, CubeMX 4.26.0 now supports TrueSTUDIO with graphics. 

Hi Richard,

When I enabled STemWin in GRAPHICS, the TrueSTUDIO selection in Project - Settings - toolchain / IDE drop list still be grey.

CubeMX 4.27.0

STM32Cube FW_F4 V1.21.0

Is just V4.26.0 support that feature and V4.27.0 don't? Or it's depend on FW?