cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.25 & Graphic

Posted on March 29, 2018 at 00:28

Why I cannot choose Graphics STemWin for STM32F769BI ???

#stemwin
1 ACCEPTED SOLUTION

Accepted Solutions
N. SANTINI
ST Employee
Posted on April 03, 2018 at 19:01

Hi,

You are fully right, some Graphics-enabled part number are not yet integrated, it is the first release of the CubeMX tool with Graphics integration it will be enhanced in the coming versions.

We are sorry for the inconvenience,

Best regards,

Nicolas

View solution in original post

5 REPLIES 5
Posted on March 30, 2018 at 06:36

0690X0000060AK5QAM.png 0690X0000060AKFQA2.png
N. SANTINI
ST Employee
Posted on April 03, 2018 at 19:01

Hi,

You are fully right, some Graphics-enabled part number are not yet integrated, it is the first release of the CubeMX tool with Graphics integration it will be enhanced in the coming versions.

We are sorry for the inconvenience,

Best regards,

Nicolas

Posted on April 03, 2018 at 19:16

Nicolas, thanks for the answer, I'll be looking forward to it

Posted on April 03, 2018 at 19:19

Nicolas,

Is there an anticipated date for which the graphics integration will be rolled out more fully?  I'm in a similar position with the STM32L496VG.  The presence of StemWin examples in the CubeL4 packages indicates the processor supports StemWin, however there is no option to enable it within CubeMX.

Regards,

Randy

Posted on April 04, 2018 at 11:37

Dear Randy,

The information I have say that v.4.26 should be released on Week22, with the L4 Graphics support and, I guess/hope, a better coverage of F4/F7 Graphics enabled part numbers.

Regards,

Nicolas