2022-05-20 7:22 AM
I have a project where I want to place the TGFX resources (images, translations, fonts) in a memory mapped QSPI flash. In this instance I have placed them in this flash via the linker (.o files) rather than using binary fonts etc.
The crash occurs generally when switching screens. I can usually switch screens successfully a number of times. Sometimes it fails after 30 screen switches, sometimes 5. I've also seen it fail when updating smaller elements. The crash also prevents the debugger (IAR / I-Jet) from stopping, so I've had no luck there. Debug log: "CPU did not stop"
I find the problem goes away if I put the TGFX fonts back in internal flash. It also goes away if I switch back to full frame buffers rather than using partial frame buffers. ( I have restrictions on ram usage, so partial frame buffers are needed)
I've given the TGFX FreeRTOS task lots of stack but that doesn't fix the problem.
I put a scope trace around the TouchGFXHAL::flushFrameBuffer(const Rect& rect) routine. It enters and exits correctly according to the trace. So it appears it's dying inside the TGFX library somewhere.
Any other ideas?
Solved! Go to Solution.
2022-05-25 5:36 AM
Update: I disabled the QSPI timeout counter as mentioned in the device errata and the problem appears to have gone away.
2022-05-23 4:57 AM
Hello Guit32010,
Can you give more information about your configuration please ?
/Osman
2022-05-23 5:32 AM
2022-05-23 5:33 AM
2022-05-25 5:36 AM
Update: I disabled the QSPI timeout counter as mentioned in the device errata and the problem appears to have gone away.
2022-05-30 2:45 AM
Hello Guit32010,
Good to hear that you resolved your problem :)
I invite you to select your answer as best answer and close the post so it would help people with the same issue to find the resolution.
/Osman