2024-10-03 10:20 AM
Hi, i'm developing a board with 7" lcd (LVDS) so i'm really hesitating about if is right to use a SN65DSI83 for this, my STM32F469IIT6 only have 2 DSI Lanes. I'm connecting the i2c lane from SN65DSI83 to i2c of STM, i just copied the circuit of cm4-baseboard-lvds-adapter (https://github.com/antmicro/cm4-baseboard-lvds-adapter) and adapted to mind. So i'm really new in this kind of applications and i don't know if i should first read the registers of SN65DSI83 and then change (i want to implement a logic that if the registers are correctly configured just read and pass but if these are not right, my stm32 write the registers) or if every time that i have turn on my circuit, the STM32 should configure all registers. So some one have a tutorial for write on the screen with the comand mode? I just make some changes but i think in the future will put only springs for my aplication. So if someone can help me with this o maybe there are some documentation that i had no reading.