cancel
Showing results for 
Search instead for 
Did you mean: 

configuration camera with 800*480 "RK043HR005" lcd with stm32f7508

Bhanu
Associate II

Hi,

I'm trying to interface 400*400 camera with 800*480 lcd display.

i have done changes for lcd as per the datasheet but still im not getting output as expected.

before i have already interfaced 400*400 camera with 480*272 lcd display it's working fine, but now I'm trying to interface with 800*480 lcd.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
KDJEM.1
ST Employee

Hello @Bhanu​,

The resolution of LTDC and SDRAM are related. You can refer to this post and check if the 128Mbit SDRAM is able to support 800x480 resolution.

I suggest you take a look at this AN4861 Application note LCD-TFT display controller (LTDC) on STM32 MCUs and STM32F7-LTDC and precisely Two programmable LTDC layers section.

I hope this helps!

Thank you.

Kaouthar.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.