Skip to main content
Adrush Rawal
Visitor II
Nov 30, 2022 8:58 AM UTC
Question

Do we need additional SDRAM/SRAM Interface for TFT Display.

Hi,

we are planning to change current LCD with 10 inch (800*600) TFT Display with TouchGFX and already we are using QSPI flash, do we need additional memory interface (SDRAM/SRAM)?

Regards,

Adrush

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
Nov 30, 2022 11:27 AM UTC

This depends on your current circumstances, e.g. the STM32 used and its size of internal RAM, the buffer strategy and the colour depth.

Your SVGA display with 800x600 pixels has a total number of 480000 pixels. At full colour resolution (RGB888) the frame buffer requirement is 480'000 * 24 = 11'520'000 bit (=1.373MB). If you also need double buffering, this value doubles again and you definitely need external RAM.

However, you can usually work with a lower colour resolution of RGB565 (65536 colours) instead of RGB888 (16 million colours), because the difference is rarely noticeable on displays with smaller dimensions. Instead of 24 bits per pixel, RGB565 only needs 16 bits, which reduces the RAM requirement by 33.3%. In your case, "only" 960'000 bits (937.5KB) are needed for a frame buffer, and 1.875MB for double buffering.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.