2023-12-08 11:00 AM
Hello,
I'm having issues trying to clear the data set from a dynamic graph in Touch GFX. Unfortunately none of the data points nor graph line are being cleared from the graph.
The graph is set to scroll as more data is added. When a "user session" is reset I would like to clear the existing data from the dynamic graph.
I would think it was as simple as calling the clear() function but I am not having any luck. Documentation says invalidation is done when clear() function is called but I have also tried adding the invalidate.
dynamicGraphVoltage.clear();
dynamicGraphVoltage.invalidate();
Thank you for any suggestions!
Solved! Go to Solution.
2023-12-14 2:21 AM
Hello @Jonathan-Halltech,
To reset the dynamic graph you just need to call the clear() function as you mentioned and you don't need to call invalidate().
If you're planning to clear the graph when user the user exits the screen, you should call the function before
2023-12-14 2:21 AM
Hello @Jonathan-Halltech,
To reset the dynamic graph you just need to call the clear() function as you mentioned and you don't need to call invalidate().
If you're planning to clear the graph when user the user exits the screen, you should call the function before