Cant find BoardConfiguration.cpp file in version 4.13.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-31 06:19 AM
I want to uncomment #define SINGLE_FRAME_BUFFER_INTERNAL to use single frame buffer in internal SRAM and i dont want TouchGFX to generate codes about FMC. Where exactly BoardConfiguration.cpp generated.
Solved! Go to Solution.
- Labels:
-
TouchGFX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-31 08:07 AM
We don't use that define with the Generator. It was mostly for BoardConfiguration.cpp's that could handle both double and single. TouchGFX Generator just calls setFrameBufferStartAddresses with one, two or three arguments. And in the case of single FB we use a specific framebuffer strategy.
/Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-31 06:30 AM
@Martin KJELDSEN​ can you help?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-31 06:55 AM
How did you generate the project? If through TouchGFX Generator / CubeMX then it's not called BoardConfiguration anymore, but TouchGFXConfiguration.cpp and its located in the TouchGFX/target/generated/ folder.
The define is there because you chose SINGLE Framebuffer in the generator (if you did) and you can just choose something else.
/Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-31 07:44 AM
Well i started the project on TouchGFX, created my GUI and generated to code to open the project from .project file with STM32CubeIDE. From the CubeMX i changed the Double Frame option to single But i couldnt find the #define SINGLE_FRAME_BUFFER_INTERNAL in TouchGFXConfiguration.cpp. Do suggest me to start project from CubeMX perspective and import to CubeIDE and lastly add GUI from .part file from scratch?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-31 08:07 AM
We don't use that define with the Generator. It was mostly for BoardConfiguration.cpp's that could handle both double and single. TouchGFX Generator just calls setFrameBufferStartAddresses with one, two or three arguments. And in the case of single FB we use a specific framebuffer strategy.
/Martin