2024-08-13 11:54 AM
I am new to the touchGFX ecosystem and I am trying to setup a touchGFX project to work with the STM32CubeIDE. I have looked at various other forum posts, youtube videos, and the touchGFX board bring up documentation to no avail. I can setup a basic project within the IDE but as soon as I add touchGFX I run into 182 undefined reference errors. I have tried starting the project in CubeMX with and without the generate under root box checked and I run into the same issues. I have noticed that by when I attempt to build the project many of my files are crossed out in the project explorer( see screenshot). I have attached a zip file of my attempt to create a blank project that just has touchGFX initialized and builds correctly.
Thanks in advance