cancel
Showing results for 
Search instead for 
Did you mean: 

Broken links in the TouchGFX documentation error has been fixed

Romain DIELEMAN
ST Employee

For your information, the TouchGFX documentation has been updated to fix the issue where you could not access links on a documentation page when opening the documentation for the first time (or when sent from a link).

The color bug for the "Tip" sections has also been fixed.

6 REPLIES 6
Martin KJELDSEN
Chief III

Thanks, Romain!

Sandy.Dahl
Associate II

Hi @Romain DIELEMAN​ !

This link is still broken to me:

https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_text_area/classtouchgfx_1_1_text_area#function-resizeheighttocurrenttext

I try to go there by clicking on resizeHeightToCurrentText from this page:

https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_text_area

Kind regards,

Sandy

Hi,

What browser are you using? I cannot seem to replicate your error. When I click on resizeHeightToCurrentText in the TextArea documentation like you did, I am sent to the right address: https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_text_area#function-resizeheighttocurrenttext.

/Romain

Sandy.Dahl
Associate II

I'm using Google Chrome. I actually couldn't manage to replicate it myself now, so maybe it's fixed.

Since your message I actually have met sometimes similar errors, but when I went back to the previous page to replicate it or refreshed the page I would not have the issue anymore. This seems like a rare error that is not critical but is still annoying. Thank you for testing again, I have forwarded this issue we will see how we can fix that.

/Romain

Michael K
Senior III

I'm still having this issue, but it only occurs at pages I land on directly from search. Tested with Chrome 86.0.4240.183 and Firefox 82.0.2 and getting identical behavior.

To reproduce: Search for the name of any API reference page, such as DataGraphWrapAndClear. Click the search result, and try clicking any of the links in the documentation section. If you refresh the page or navigate to the URL directly it behaves as normal.

From search, a link turns into:

https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_data_graph_wrap_and_clear/classtouchgfx_1_1_abstract_data_graph_with_y

When navigated to directly, a link turns into:

https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_abstract_data_graph_with_y