cancel
Showing results for 
Search instead for 
Did you mean: 

Application template for stm32 not loading in touchgfx, showing error...

KMitt
Associate II

Not able to load any templates except the windows template.

8 REPLIES 8
Martin KJELDSEN
Chief III

Hi @KMitt​,

Can you please attach your log file?

/Martin

Thanks for the reply...there was no log file generated because it can't load the template. It finally worked when I changed the directory location.

Can you put links for tutorials on modifying the code for adding different buttons (especially sliders).

Also what type of compiler will be good if I don't have visual studio

Hi,

If you don't have visual studio TouchGFX comes with gcc projects out of the box. (Also available if you create your TouchGFX projects through CubeMX/CubeIDE).

I suggest you check out these resources to get started with adding widgets: https://touchgfx.zendesk.com/hc/en-us/categories/200529271

/Martin

Hi @KMitt​,

Any progress on this?

/Martin

Thanks for the reply. I checked the tutorials but it is not much help.

Can you tell me how to use input from slider button for changing the text fields.

Kumud

KMitt
Associate II

Hello

Can you look into this. The slider button is causing problems. I think the issue is from software side

please check

You have no background.

Just back from vacation now, sorry for the late reply. When the knob leaves an area of the screen because you're dragging what's left behind must be redrawn - But there's nothing there.