2019-04-05 1:33 AM
Is it possible to animate standard objects (e.g. box, circle, shapes, containers, etc.) with EasingEquations?
For example take a circle with a small radius and a thin line and zoom it to a bigger radius and thick line smoothly in 1 second?
Solved! Go to Solution.
2019-04-10 12:29 AM
Hi @WPrec,
Instead of coming up with a new example, i'd like to show you how this can be done using what we call "Mixins", that you can select for a widget (e.g. a box) through the designer. For the MoveAnimator mixin (touchgfx/mixins/MoveAnimator.hpp) it uses an easing equation to calculate both x and y and uses the moveTo() method to move and invalidate the widget. If we were to simply modify this code to also set a size this clearly shows how animating the size of a widget over time can be done.
So, you could create your own mixin (just copy the MoveAnimator) and do something like the following:
/**
* @fn void MoveAnimator::nextMoveAnimationStep()
*
* @brief Execute next step in move animation.
*
* Execute next step in move animation and stop the timer if necessary.
*/
void nextMoveAnimationStep()
{
...
T::moveTo(moveAnimationStartX + deltaX, moveAnimationStartY + deltaY);
// Besides moving, also set width and height to some value returned by the easingequation
T::setWidth(deltaX);
T::setHeight(deltaY);
T::invalidate();
moveAnimationCounter++;
}
....
}
Create an application with a moveanimator (interaction on screen-entry) to get a feel for what code gets generated and how to use it.
Best regards,
Martin
2019-04-08 2:15 AM
Hi @WPrec,
Yes, through Mixins in the bottom right hand of the designer. You can add a MoveAnimator or FadeAnimator, for isntance, to your box. It will then be available through interactions that you can then specify an easing equation for.
Best regards,
Martin
2019-04-08 4:53 AM
Hi Martin,
I saw the MoveAnimator and FadeAnimator and they work well.
But the intention is, to change object values (e.g. width, height, line width, color or something else) with EasingEquations?
2019-04-08 6:34 AM
Ah, okay. That's not supported right now through the designer. Sorry! You could do it in pure code by making your widget tick-aware and then just getting your values from an easing equation over time. Does that make sense?
If i get some time i could create an example .
/Martin
2019-04-08 11:05 PM
Thank you Martin.
An example would be great!
2019-04-08 11:51 PM
Okay, i'll try to get it done this week. I just had a talk with some guys at the office about creating a better framework for animations. Right now it's kind of hidden away through a combination of mixins and interactions - And not present for some things like resizing widgets.
If you want to resize an image you could always use ZoomAnimationImage which uses a scaleable image / texturemapper.
2019-04-10 12:29 AM
Hi @WPrec,
Instead of coming up with a new example, i'd like to show you how this can be done using what we call "Mixins", that you can select for a widget (e.g. a box) through the designer. For the MoveAnimator mixin (touchgfx/mixins/MoveAnimator.hpp) it uses an easing equation to calculate both x and y and uses the moveTo() method to move and invalidate the widget. If we were to simply modify this code to also set a size this clearly shows how animating the size of a widget over time can be done.
So, you could create your own mixin (just copy the MoveAnimator) and do something like the following:
/**
* @fn void MoveAnimator::nextMoveAnimationStep()
*
* @brief Execute next step in move animation.
*
* Execute next step in move animation and stop the timer if necessary.
*/
void nextMoveAnimationStep()
{
...
T::moveTo(moveAnimationStartX + deltaX, moveAnimationStartY + deltaY);
// Besides moving, also set width and height to some value returned by the easingequation
T::setWidth(deltaX);
T::setHeight(deltaY);
T::invalidate();
moveAnimationCounter++;
}
....
}
Create an application with a moveanimator (interaction on screen-entry) to get a feel for what code gets generated and how to use it.
Best regards,
Martin
2019-04-23 6:00 AM
Hi Martin,
sorry for the late reply - but the job goes on.
I tried this with a circle and changed the radius and startArc and endArc and it works.
Thank you very much.
2019-04-29 12:34 AM
Hi @WPrec,
That's great! You're welcome.
Best regards,
Martin