2023-02-24 04:52 AM
Hi,
I've inherited a project which was designed using the STM32F746-G Discovery board as a reference design.
It uses an RK043FN48H display with touch, same as what is used on the discovery board. The TouchGFX library is used for the graphics. The BSP for the discovery board is used in our design.
We've recently discovered that this display is going obsolete due to obsolescence of the FT5336 CTP IC.
Our software uses the drivers written by ST for this display and CTP chip and we want to avoid having to write our own drivers. The recommended alternative uses the GT911 CTP but it doesn't look like ST have written any drivers for this?
Is there a recommended 4.3" display that would be software compatible with existing code written for the RK043FN48H. Or alternatively, is there a different 24-bit RGB display that uses a CTP IC which has pre-written drivers which could be easily imported into our codebase without having to do a rewrite?
Thanks!