About SDRAM on STM32F746 microcontroller
Hi I am new in ST microcontrollers, I'm working with NXP microcontroller (LPC54018) and I would like migrate our project to ST microcontroller. The first reason is the use of TouchGFX designer, the second one is when it needs to access to SDRAM, sometimes it get slowly. To migrate the project we need to know if this environment could do better the use of SDRAM driver.
The questions are:
*Is there a posible that it won't happened(sometimes is visible the image painting process) with this micro?(using TouchGFX designer)
*The use of SDRAM is performed automatically? If not, are there some examples about use of SDRAM?