2018-01-10 5:51 AM
Hi there,
I wrote a serial protocol to exchange data between MCU and a PC.
This protocol provides a checksum to verify data integrity.
At the moment I use a simple sum of each byte but I think that the use of CRC peripheral could be an improvements.
Unfortunately the CRC peripheral requires a uint32_t buffer but my payload is an uint8_t.
Casting the uint8_t to uint32_t is a problem because the CRC will be wrong because on the PC side.
I computed the CRC as byte (from serial interface)but I computed the CRC on MCU as word (due to cast uint8_t to uint32_t ).
/* This is my packet structure */
*/
typedef struct PROTOCOL_Packet
{
uint8_t header;
uint16_t length;
uint8_t payload[128];
uint32_t checksum;
} PROTOCOL_Packet_t;
/* This is my routine to compute the CRC: */
if( CRC_Calculate( (uint32_t*)pkt->payload.bytes, (uint32_t)(*pkt).length, &pkt->checksum ) == APP_TRUE )
{
SERIAL_Write( (uint8_t*)pkt, pkt->length + 7 );
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
/* Where CRC_Calculate is: */
uint8_t CRC_Calculate( uint32_t* buffer, uint32_t bufferLen, OUT uint32_t* crc32)
{
*crc32 = HAL_CRC_Calculate( &hcrc, buffer, (bufferLen/4) );
return TRUE;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
I can't change the type of my payload to uint32_t because on the PC side I want to avoid byte manipulation to retrieve the uint32_t back from bytes.
Any suggestion?
Thanks in advance
#crc32 #stm32f1032018-01-10 10:01 AM
The STM32F1 CRC generator has a fixed polynomial, shift direction, byte order and width, this is not terribly consistent with endian ordering of the PC or STM32.
The F3 and some F0 have a more flexible solution.
Do the computation in software. Or byte stuff on the PC side, where the operations are of trivial code on a PC running at >3GHz
//******************************************************************************
uint32_t CRC32(uint32_t Crc, uint32_t Size, uint8_t *Buffer)
{ while(Size--) {static const uint32_t CrcTable[] = { // 0xEDB88320 polynomial, right shifting -
mailto:sourcer32@gmail.com
0x00000000,0x1DB71064,0x3B6E20C8,0x26D930AC,0x76DC4190,0x6B6B51F4,0x4DB26158,0x5005713C, 0xEDB88320,0xF00F9344,0xD6D6A3E8,0xCB61B38C,0x9B64C2B0,0x86D3D2D4,0xA00AE278,0xBDBDF21C };Crc = Crc ^ (uint32_t)*Buffer++; // Consume a byte at a time
Crc = (Crc >> 4) ^ CrcTable[Crc & 0x0F]; // Two rounds of 4-bits
Crc = (Crc >> 4) ^ CrcTable[Crc & 0x0F]; }return(Crc);
}//******************************************************************************