cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030F4P6 option byte programming

leo12345678
Associate II

Can recognize the chip, but can not burn and read the flash problem. In this case, is the chip broken or the chip locked?

There is also a case that the chip can be identified as burning, but it cannot run the normal working program

2 REPLIES 2
TDK
Super User

Is this a genuine programmer? The serial number "123456" is suspect.

TDK_0-1742559782658.png

Can you connect over SWD?

If you feel a post has answered your question, please click "Accept as Solution".

@TDK wrote:

Is this a genuine programmer? 


@leo12345678 - see:

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/ta-p/49471

In particular:

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/tac-p/703663/highlight/true#M965

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.