2022-05-18 09:36 AM
I wish to try the TFM application on my B-U585I-IOT02A demo board. But the support for STM32CubeIDE has disappeared in FW_v1.1.0. Is there any reason for that, or can I copy the project from patch_cube5_v.1.0..2, though the source files have significantly changed since then ?
Regards
2022-05-27 06:34 AM
Hello @ELuca.2 and welcome to the community,
I checked the release note under this path :
STM32Cube/Repository/STM32Cube_FW_U5_V1.1.0/Release_Notes.html
in the "Known Limitations" section they mention that TFM applications are not supported with MDK-ARM and STM32CubeIDE toolchains, also in the "Projects" section they mention that they update the TFM applications for new versions of middlewares with Security features and integration of STSAFE Middleware on B-U585I-IOT02A board
Mohamed Aymen
2022-09-06 08:04 AM
Hello,
Is there a plan to release STM32CubeIDE projects for TMF on U858 in the near future?
Regards