2020-10-08 5:48 PM
Dear st team,
I have a development issue when running TFM example application at STM32L562.After download the tfm_s_enc_sign.bin through ymodem,print error log"[ERR] Image in the secondary slot is not valid!" when secure boot .ALL other 3 bin(tfm_s_sign.bin,tfm_ns_sign.bin,tfm_ns_enc_sign.bin) download success.
I follow the document UM2671 chapter 11.4 Download a new firmware image.
The project is en.stm32cubel5_v1-3-0.zip,file:Projects\STM32L562E-DK\Applications\TFM
Steps to reproduce:
Reason:
1.hash verify not pass because after decrypt, the image not same with origin image.log as below:
=====================================================
[INF] verify counter 0 1000000 1000000
[INF] counter 0 : ok
[INF] hash256 : 54, cc, 2c, 4c, 97, b5, 55, 68,
[INF] hash256 buf : cd, 76, a3, a1, cb, 1, 4d, bc,
[ERR] Image in the secondary slot is not valid!
======================================================
Does anyone know what I'm doing wrong?
Thanks in advance!
2020-10-14 10:00 AM
Hello,
So, apparently you didn't change anything and just compiled and run the example ?
What IDE/compiler did you use?
Did you notice any warning during compilation ?
Best regards
Jocelyn
2020-10-20 2:34 AM
Thanks for your answer.yes,i didn‘t change anything at all.
I found the reason after debug:decrypt error when call function mbedtls_aes_crypt_ecb(). Because define MBEDTLS_AES_ALT, it use hardware to decrypt the image.After undefine MBEDTLS_AES_ALT, it use mbed-crypt lib to decrypt the image and then decrypt right.
I think there's something wrong with the decrypt api in aes_alt.c, but i didnt have enough time for more deep debug.hope you can give some comments about it
Thanks in advance!
2020-11-17 5:25 AM
Hello,
I'm sorry I missed your answer.
So, you mean you have a STM32L562 and not able to hardware for decryption ?
Only explanation I could have is that your chip is not a L562 but rather a L552.
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.