2023-03-24 11:49 AM
Hi there. Before attempting any password locking on my STM32575, I read the password lock location and it returned all zeroes like so
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x40022020
0x40022020 : 00000000
After setting the PW, it now returns non zero like so
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x40022020
0x40022020 : 000C0000
I've tried disabling the PW, writing to all zeroes and writing it to all FFs, but I can't get back to the point where all zeroes are returned. Can you advise how to get to that state?
thanks in advance
Paul
Solved! Go to Solution.
2023-03-27 5:25 AM
Hello F Belaid
I did figure this issue out. I needed to reset both RDP1 and RDP2 passwords. Thanks for reaching out
2023-03-27 5:23 AM
Hello @PChoq.780
Do you mean STM32U575? If yes, how do you read the password lock location?
Note that:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-27 5:25 AM
Hello F Belaid
I did figure this issue out. I needed to reset both RDP1 and RDP2 passwords. Thanks for reaching out
2023-03-27 5:27 AM
Thank you for your feedback.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.