2020-06-17 7:24 AM
I have made a FUOTA project and I want to add security to it. I found SBSFU but I see that they must connect the ship in order to update it, and that's not what I want.
So my question : is it possible to do a FUOTA with a SBSFU example ? is so how ?
2023-01-18 2:05 AM
Hi @Moughit,
I suppose by FUOTA you mean field upgrade over the air. But I don't really understand "connect the ship" .
However generally it's possible to change the way the new FW is loaded, including OTA. However details vary depending on what particular STM32 you plan to use. On U5 and for example WL the SBSFU are completely different SW.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.