2022-01-21 3:59 AM
2022-01-21 4:12 AM
I tried to disable the JTAG by setting the RDP to level 2. It has disabled the JTAG access But I have flashed an application in internal flash which allows me to read and write internal flash using UART Now I am not able to read or write the internal flash. Will the RDP level 2 stop the access(read/write) to internal flash by the internal program also? I don't know what should I do now?
Here is what the datasheet says: In RDP level 2, I understand that flash read and write should be disabled via JTAG but Flash read or write should be allowed by an internal application/program stored in the internal flash.
2022-01-21 4:13 AM
STM32F4 is used in this project
2022-01-21 6:38 AM
Can you print out the option bytes from your program? Any sector-level WRP are set?
> I don't know what should I do now?
Replace the MCU.
2022-01-21 9:06 AM
Check any errata doc for the chip.
If you are not able to access memory through usart, maybe there is something else that is wrong in the code. Use a blinky to check your code is not in exception mode.Maybe if using the stlink vcp doesn t work unless the debug is active?
2022-01-24 4:44 PM
> Will the RDP level 2 stop the access(read/write) to internal flash by the internal program also? I don't know what should I do now?
No, it does not. See reference manual:
I'm sure you've got something else going on there, which you're not going to be able to solve let alone debug due to RDP level 2.