2021-05-14 3:20 AM
Hi all,
I've downloaded the package 'STM32CubeExpansion_SBSFU_V2.4.0' and I've opened, using STM32CubeIDE (Version: 1.6.1), the project STM32WB55RG_Nucleo_2_Images_SECoreBin.
I'm not able to compile the project because I've the following error:
arm-none-eabi-gcc -mcpu=cortex-m4 -c -x assembler-with-cpp -MMD -MP -MF"Application/SW4STM32/se_key.d" -MT"Application/SW4STM32/se_key.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -o "Application/SW4STM32/se_key.o" "C:/progetti/INFOBOX_3.0/Micro/download/en.x-cube-sbsfu/STM32CubeExpansion_SBSFU_V2.4.0/Projects/P-NUCLEO-WB55.Nucleo/Applications/2_Images/2_Images_SECoreBin/SW4STM32/se_key.s"
arm-none-eabi-gcc -mcpu=cortex-m4 -c -x assembler-with-cpp -MMD -MP -MF"Application/SW4STM32/startup_stm32wb55xx_cm4.d" -MT"Application/SW4STM32/startup_stm32wb55xx_cm4.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -o "Application/SW4STM32/startup_stm32wb55xx_cm4.o" "C:/progetti/INFOBOX_3.0/Micro/download/en.x-cube-sbsfu/STM32CubeExpansion_SBSFU_V2.4.0/Projects/P-NUCLEO-WB55.Nucleo/Applications/2_Images/2_Images_SECoreBin/SW4STM32/startup_stm32wb55xx_cm4.s"
arm-none-eabi-gcc -o "SeCoreBin.elf" @"objects.list" -l:libSTM32CryptographicV3.0.0_CM4_GCC.a -mcpu=cortex-m4 -T"../stm32wb55xx_flash_cm4.ld" --specs=nosys.specs -Wl,-Map="SeCoreBin.map" -Wl,--gc-sections -static -Wl,--start-group -l:libSTM32CryptographicV3.0.0_CM4_GCC.a -Wl,--end-group -L../../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32WB/Lib -Xlinker -L ../../../../Linker_Common/SW4STM32 --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: SeCoreBin.elf section `.rodata' will not fit in region `SE_ROM_region'
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: region `SE_ROM_region' overflowed by 401 bytes
collect2.exe: error: ld returned 1 exit status
make[1]: *** [makefile:68: SeCoreBin.elf] Error 1
make: *** [makefile:61: all] Error 2
"make -j8 all" terminated with exit code 2. Build might be incomplete.
What's the problem? How can I resolve it?
Regards,
Giampietro
2021-05-28 8:41 AM
Hello @Community member,
This looks similar to the case reported in this question. Try the workaround suggested by Jocelyn here.
Chahinez.
2021-06-24 1:06 PM
Hello,
You can reduce the overflow size by playing with the gcc optimization flags.
If that is not enough, you can change the size of the region. Please see X-CUBE-SBSFU integration guide AN5056, chapter 6.2.
Regards
Henke