cancel
Showing results for 
Search instead for 
Did you mean: 

I have downloaded the X-CUBE-SBSFU V2.4.0 and build project NUCLEO-G071RB. It works and can download firmware from Tera Term's ymodem send. Can we use only Tera Term? Do any other tools be used for download firmware?

EEdwa.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
18 REPLIES 18

Hi Arno,

I try to use your setting, but still failed.

My sb version is:

sb --ver

sb (lrzsz) 0.12.21rc

Could you share your sb version?

Thank you

Hi Jocelyn,

I have try to activate MINICOM_YMODEM flag, but failed.

The error logs are the following,

Could you help how to solve the problem?

= [SBOOT] System Security Check successfully passed. Starting...
 
 
======================================================================
=              (C) COPYRIGHT 2017 STMicroelectronics                 =
=                                                                    =
=              Secure Boot and Secure Firmware Update                =
======================================================================
 
 
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
          INFO: A Reboot has been triggered by a Software reset!
          INFO: Last execution detected error was: FW too big.
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK USER FW STATUS
          No valid FW found in the active slots nor new FW to be installed
          Waiting for the local download to start... 
= [SBOOT] STATE: DOWNLOAD NEW USER FIRMWARE
          File> Transfer> YMODEM> Send CCCCCCCCCCCCCCCCCCCCC

mine's the same: sb (lrzsz) 0.12.21rc

Your output says `INFO: Last execution detected error was: FW too big.`

Have you changed anything to the userapp?

No, I don't change anything to the userapp.

I have try the below settings, but both failed.

  1. If I activate MINICOM_YMODEM flag, I must use setting "/usr/bin/sb -vv", then will start download.
  2. If I deactivate MINICOM_YMODEM flag, I must use setting "/usr/bin/sb -vv -k", then will start download.

Hi EEDwa,

are you using SBSFU 2.4.0 version?

I remember, but not 100% sure, that this FW too big was a "bad" error code in previous SBSFU version.

Also, the support of MINICOM came with the 2.4.0

Best regards

Jocelyn

Hi Jocelyn,

Yes, I use SBSFU 2.4.0.

But still failed even if I activate MINICOM_YMODEM flag.

Hi EEdwa,

could you please tell in which environment you are working?

I could try to reproduce your issue on a virtual machine.

Best regards

Jocelyn

Hi Jocelyn,

My OS is Ubuntu 16.04.7 LTS

Thank you.

Hi EEDwa,

I could reproduce your issue after installing this version on a virtual machine.

I'll try to understand what happens.

I used a STM32L476 as example.

Behaviour is actually different between SBSFU loader and application loader.

On SBSFU loader, using -k (for 1kbytes download) fails immediately. Removing -k, it starts transfering very slowly 1 sector of 128 B/sec and fails at the end.

Using application side loader, the transfer is occuring quite fast then stops and send 2or 3 more sectors before failing.

I suspect issues related to timeout.

Best regards

Jocelyn

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.