2020-12-27 07:16 AM
Hello
In STM32 Crypto Library, there are function "AES_CMAC_Encrypt_Init", "AES_CMAC_Encrypt_Append" and "AES_CMAC_Encrypt_Finish" to calculate the authentication code of a plain text.
How can this be done on STM32WB using the CRYP peripheral (HAL driver) ?
Best regards
Paul
2020-12-27 07:45 AM
The STM32W series parts tend to be built by a different group within ST, support is often rather limited. If you are a commercial user of these parts I'd suggest rattling the tree starting with your sales rep and FAEs
The general problem with the HW CRYPT/HASH implementations is they are single context, non-thread safe. You will have to look at the implementation details, especially size and alignment expectations, and perhaps hold small buffers of pending data when the size/alignment requirements aren't met by the "append" requests that arrive.
I would look at the HAL CRYP examples under CubeWB (or whatever), but it's not my part and I can't spend time on.
Related topics you've posted, the audience here is pretty slim (support / abandonment issues)
@ST Community if ST wants their wireless products to be used the support staff need to start showing up. Large customers have deeper rosters of engineers, and should need less help, answering forum problems has much further reach and if done properly it identifies issues early, and inspires potential customers to have confidence.
2020-12-27 09:05 AM
Hi Tesla
Thanks for the reply. I like specifically your last paragraph ;)
The sample software in the distributed FW package is really "light" concerning CRYP peripheral.
The best for customers (small companies/startups) would be if there is a HW version of STM32 crypto library on STM32WB.
BR
Paul
2020-12-27 10:00 PM
I don't know about WB, but for STM32H75x had to edit stm32h7xx_hal_cryp.c manually to enable init-append-finish workflow.
It was not so hard, but could find better use for my time...
-- pa