cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, if I integrate the external STSAFE-A110 crypto module on my board, does it give STM32 a higher level than the level-3 on SESIP?

SShoh.1
Associate
 
1 REPLY 1
Benjamin BARATTE
ST Employee

Hi @SShoh.1​ 

STSAFE-A110 is certified secure element which provides a smart card like level of protection of cryptographic assets to your application only.

Adding a secure element doesn't grant higher level of SESIP certification as the whole device shall be audited.

For STM32 product, the target of the evaluation is SESIP Level 3 on recent product only. If you target higher level, it's up to you to fill the gap between the Level 3 and Level 4

Best Regards,

Benjamin